Web Browser general properties

The following table shows settings on the
General
tab.
Setting
Description
Show address bar
Select to use the standard address bar, including Refresh, Stop, Forward, and Back.
If selected, the tags or expressions on the
Connections
tab are ignored.
Initial URL
Enter the URL of the site you want to set as the initial page.
If not specified, the default address is the same as the home page of your Internet browser.
Use parameter placeholder for initial URL
Select to use parameter placeholders in the initial URL.
The parameter placeholder can be substituted with a literal string at runtime, for example,
#1
=
www.rockwellautomation.com
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal