Connections for the Web Browser object
The following table shows the connections to control the operation of the Web Browser object at runtime.
Connections | Descriptions |
|---|---|
URL | Required if Show address bar is not selected.This connection specifies the URL of the webpage to be shown in the control. The connection can be a fixed string (for example,
"http://www.rockwellautomation.com/") or a memory or direct reference
string tag. A string tag would contain the URL of the webpage to be shown in the
control. |
Back | Optional. A zero to non-zero transition will navigate backward one item in web browser's history list. The connection is read-only. The connection data type is Boolean. |
Forward | Optional. A zero to non-zero transition will navigate forward one item in web browser's history list. This connection is read-only. The connection data type is Boolean. |
Stop | Optional. A zero to non-zero transition will cancel any pending navigation or download operation and stop any dynamic page elements, such as background sounds and animations. This connection is read-only. The connection data type is Boolean. |
Refresh | Optional. A zero to non-zero transition will reload current webpage. This connection is read-only. The connection data type is Boolean. |
Provide Feedback