Create a vertical slider

Use the
Vertical Slider
option on the
Animation
menu to create a graphic object that can control the value of a specified tag. With vertical slider animation, you define a path for the object, then use the mouse to move the object vertically along its path. The pixel position of the object is translated into a value that is written to the tag.
A tag that has values input by slider animation can be used in an expression to attach animation to another object or group of objects. If the tag value is changed externally, the position of the slider will change as well.
Both vertical and horizontal slider animation can be attached to the same object.
To create a vertical slider:
  1. In
    FactoryTalk View Studio
    , in the
    Graphics
    editor, draw an object that is to be the slider. It is also useful to draw an object, for example a line or rectangle, that represents the path the slider will move along.
  2. Right-click the object and select
    Animation
    >
    Vertical Slider
    .
  3. In the
    Vertical Slider
    tab, specify the following properties.
    • tag
    • expression range
    • vertical offset
      TIP:
      You can also use the Object Smart Path to define the range of motion for the slider.
      The value of the tag will be proportional to the vertical position of the slider on the path defined by the minimum and maximum vertical offsets. If the object is halfway along the path, the value of the tag will be halfway between the minimum and maximum tag values.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal