Vertical Slider tab

The following table shows options in the tab.
Options
Description
Tag
Specify the name of the tag to which values will be written.
Expression range
Set minimum and maximum values for the tag
Use tag's min and max property values
If you have specified a tag in the Expression box, click this button to use the tag's minimum and maximum values to define the range of values. This option only applies to tags for which minimum and maximum can be defined, such as HMI tags.
Use constant
To use constant numeric values to define a range of values, click this button and specify values for minimum and maximum.
Read from tags
To define the range of values using one tag's value for the minimum and another tag's value for the maximum, click this button and then specify a tag for minimum and another for maximum. Using this option, when the animation for an object is started, the tags' values are read once to set the minimum and maximum values. The tags are not read again after, nor are the minimum and maximum values changed.
Vertical offset (Pixels)
Offset refers to the position of an object in relation to some starting point. When you select an object, its position is considered to be the starting point, which gives it an offset of 0.
At minimum
Specify the offset, in pixels, of the beginning of the slider's path, or select and move the slider to this position. Click the check box.
At maximum
Specify the offset, in pixels, of the end of the slider's path, or drag the object to this position. Click the check box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal