Create a scale
Use the scale object to draw a line with tick marks on it.
The scale can be used as a ruler or measuring guide. For example, you can place the scale next to a bar graph, with text labels at the top and bottom, to illustrate the range of the bar graph.
To draw a scale:
- InFactoryTalk View Studio, in theGraphicseditor, selectObjects>Gauge and Graph>Scale, or click the scale icon in the toolbox.
- Press the mouse button and drag the mouse diagonally to draw the scale.
- When the scale is the intended size, release the button.
- In theScale Propertiesdialog box, specify how you want the scale to look.
Provide Feedback