Example: Use a scale

In this example, the scale object helps in visually determining the speed of a conveyor as depicted by a bar graph.
Create a scale and change the number of minor ticks to 9, and the back style to transparent. Place the scale on top of a bar graph. As the bar graph fill changes the value it represents can be determined by using the scale ticks as markers.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal