Work with timer steps
If the recipe on the batch list contains one or more Timer steps, you can reset the Timer step or force it to complete. The batch must be in MANUAL mode, which places the Timer step into O-AUTO mode.
TIP:
The Timer step must be in the RUNNING state for Timer Complete and the RUNNING or HELD
states for Timer Reset.
Provide Feedback