Force a timer step to complete

  1. In the Batch List view, double-click the batch that contains a Timer step. The batch opens in the Procedure view.
  2. When the Timer step becomes active, place the batch in MANUAL mode.
  3. Select the Timer step in the SFC or Table view, and then click the
    Timer Complete
    button.
    When a Timer step is in the RUNNING state and receives a Timer Complete command the Timer step will transition to the COMPLETE state. If a Timer Complete command is issued and the command is no longer valid, due to a change of state for example, the command is ignored.
    TIP:
    If the logged in user does not have permission to send the Timer Complete or Timer Reset commands, the commands will not be enabled even if the Timer step is in the proper mode and state.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal