Reset a timer step

  1. In the Batch List view, double-click the batch that contains a Timer step. The batch opens in the Procedure view.
    ePro_timer_step
  2. When the Timer step becomes active, place the batch in MANUAL mode.
  3. Select the Timer step in the SFC or Table view, and then click the
    Timer Reset
    button.
    When a Timer step in the RUNNING or HELD state receives the Timer Reset command the ELAPSED_TIME report will be reset to 0. If the Timer step is configured as a COUNT_DOWN timer the REMAINING_TIME report will be reset to the setpoint value. If the Timer Reset command is issued and the command is no longer valid, due to a change of state for example, the command is ignored.
    TIP:
    If the logged in user does not have permission to send the Timer Complete or Timer Reset commands then the commands will not be enabled even if the Timer step is in the proper mode and state.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal