How PhaseManager works
PhaseManager
PhaseManager™
features work together to provide a seamless workflow that improves the designing,
troubleshooting, and commissioning phases of the development life cycle. This discussion
includes some background information about the components of FactoryTalk Batch
systems and how FactoryTalk Batch
terminology and concepts are implemented in FactoryTalk Batch
and Logix Designer
. In a
FactoryTalk Batch
system using PhaseManager
, the FactoryTalk Batch
Server provides batch control, including recipe
execution, allocation and arbitration of equipment, binding of resources, and generation of
journals. Use FactoryTalk Batch Equipment Editor
and FactoryTalk Batch Recipe Editor
to configure the FactoryTalk Batch
system. Use Logix Designer
to program the phase logic code that
defines the behavior of equipment phase states, including Running, Stopping, Aborting,
Holding, Restarting, and Resetting. PhaseManager
links a phase in FactoryTalk Batch Equipment Editor
to a corresponding equipment phase and its phase
logic in Logix Designer
.Provide Feedback