PhaseManager
PhaseManager™
is a collection of features that integrates the FactoryTalk®
Batch software with the Studio 5000 Logix Designer
™ application and the Logix 5000™
family of controllers. The integration of
these products simplifies the configuration and maintenance of the FactoryTalk Batch
automation system, provides a superior means of
communication between the FactoryTalk Batch
Server and the Logix 5000
controller, and significantly reduces the
programming effort required to develop the phase logic code that resides in the Logix 5000
controller.Provide Feedback