Data from FactoryTalk Batch Server

IMPORTANT:
The information in this section only applies to programming phase logic for
PhaseManager
phases assigned to a
Logix5000
CIP data server.
PhaseManager
phases created with a
Logix5000
CIP data server, use the PXRQ instruction provided in
Logix Designer
as a means for the phase logic to request data or services from the
FactoryTalk Batch
Server. Much of the work involved with writing phase logic centers around defining a sequence of steps for a phase. Some of these steps require interaction with the
FactoryTalk Batch
Server. For example, the phase logic for a charge phase may perform these steps to add material to a unit:
Steps requiring interaction with the FactoryTalk Batch Server
STEP
Interacts with
Download target amount
FactoryTalk Batch
Server
Acquire pump PM102
FactoryTalk Batch
Server
Reset totalizer
Basic Control
Open valve FV101
Basic Control
Start pump PM102
Basic Control
Wait for totalizer to reach target
Basic Control
Stop pump PM102
Basic Control
Close valve
Basic Control
Release pump PM102
FactoryTalk Batch
Server
Unload actual amount
FactoryTalk Batch
Server
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal