Generate an electronic signature request
During batch execution, phase logic can issue a request to the
FactoryTalk Batch
Server to generate a Signature Request. Each Signature Template is assigned a unique ID, which is a positive integer. Requests to generate a Signature specify the desired Signature Template ID. Configure the PXRQ instruction in Logix Designer
to generate an electronic signature request:External Request | Data Value Array Element | Value |
|---|---|---|
Generate E Signature | DINT[0] | signature template ID |
DINT[1] | Defines if signature is able to be canceled: 0 = No non-zero = Yes |
Provide Feedback