Manually restart the FactoryTalk Batch Server

This task explains how to manually restart the
FactoryTalk® Batch
Server in case of a system or service failure.
If the
FactoryTalk Batch
Server service fails, then you need to manually restart the service using the
FactoryTalk Batch
Service Manager.
  • A Warm Restart or Warm All Restart of the batch server attempts to restore batches (that were on the batch list when the server previously terminated) to the batch list with active transitions in the HELD state, and recipe procedures in MANUAL mode. These restart types require operator interaction.
  • A Hot Restart attempts to restart the Batch server in a mode where it attempts to restore all batches into their last known state, including transition states and recipe modes, without any operator interaction.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal