Manually do a Hot Restart of the FactoryTalk Batch Server
This task explains how to manually do a Hot Restart of the
FactoryTalk® Batch
Server in case of a system or service failure.If the
FactoryTalk Batch
Server service stops, then you need to manually restart
the service using the FactoryTalk Batch
Service Manager. A Hot Restart attempts to
restore the batches in the last known state they were in, including transitions and modes of
recipe procedures, without any operator interaction.To do a Hot Restart of the
FactoryTalk Batch
Server:- In , selectBatch Service Manager. TheBatch Service Manageropens.
- SelectHot Restartas the startup type.
- SelectStart/Continueto start the service. Wait for the status to change to RUNNING and the light to turn green.
- OpenFactoryTalk Batch View.
- Batches on the batch list before the failure are still on the batch list. Inspect the batches to verify they are progressing as expected.
Provide Feedback