Supported command-line operations
FactoryTalk Action Manager
allows you to use command-line parameters to perform these operations without interacting with the user interface:- Back up the configuration to a BAK file
- Restore the configuration from a BAK file
Provide Feedback