Workstation

The following table explains the properties and status of workstations and their meanings.
Item
Description
Name
Shows the workstation name.
Host Name
Shows the host name of the workstation.
Description
Shows the information of the workstation.
Operations
Shows the operations that can be performed, including:
  • Backup
    Back up the configuration on the configuration user interface to a BAK file.
  • Restore
    Restore a BAK file to the configuration user interface. The restored configuration will overwrite the previous configuration in the configuration user interface.
Status
Shows the synchronization status between the configuration user interface and the runtime service, along with the timestamp of the last saved configuration. The status includes:
  • saved
    Connected, saved
    The connection is successful, and the configuration has been saved.
  • not saved
    Connected, not saved
    The connection is successful, and the configuration has not been saved.
  • disconnected
    Disconnected
    Unable to establish the connection.
Log Configuration
Defines the minimum logging level. All log information is displayed on the Log tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal