Log tab

The
Log
tab displays everything that happened in
FactoryTalk Action Manager
. The following table explains the items on the
Log
tab and their meanings.
Item
Description
Refresh
Refreshes the log list.
Export
Exports the filtered log information to a CSV file.
Severity
Shows the severity of the log, including:
  • Error
    Indicates a problem that occurred.
  • Warning
    Indicates a condition that might cause a problem in the future.
  • Audit
    Indicates the project configuration was deployed and the configuration file was saved.
  • Information
    Indicates operations were performed in FactoryTalk Action Manager, such as running actions or updating wall-clock.
Tip:
To define the desired level of logging, go to
Configuration
tab >
Workstations
>
Log Configuration
.
Message
Shows the description of the log.
Provider
Shows all related workstations, triggers, and tasks in this log.
Timestamp
Shows the server computer time that the log was generated.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal