Components in the FactoryTalk Action Manager window
The following table explains the components in the
FactoryTalk Action Manager
window and their meanings.Item | Description |
|---|---|
![]() | Shows the current user. Select to sign out FactoryTalk Action Manager . |
Configuration tab | Allows you to:
|
Server Status tab | Shows the general information of FactoryTalk Action Manager . |
Log tab | Shows the log information. |
![]() | Opens the FactoryTalk Action Manager Help. |
Save | Saves changes made to the configuration so the service will use them. |
Exit | Selects to exit FactoryTalk Action Manager . |
TIP:
To zoom in or zoom out the
FactoryTalk Action Manager
window, use Ctrl
+rotate the mouse wheel on any tab.Provide Feedback