Connection view
Use the
Connection
view to define controller-to-device behavior. Use the Connection
view to:- Select a requested packet interval.
- If supported, choose a Unicast or Multicast connection over EtherNet/IP
- If supported, choose a scheduled or unscheduled connection over ControlNet.
- Choose to inhibit the device.
- Configure the controller so that a loss of connection to this device causes a major fault in the controller.
- View connection faults.
TIP:
The data in the
Connection
view comes directly from the controller. The Connection
view displays information about the condition of the connection between the controller and the device.Provide Feedback