Points view parameters (input device)
The
Points
view includes these parameters.
TIP:
The available parameters depend on the device being configured. Parameters that do not apply to the device are hidden.
Parameter | Description |
|---|---|
Point | Indicates the point number to which this configuration applies. |
Point Mode | Determines the input mode for the associated point.
|
Test Source | Specifies the output terminal associated with the pulse test. The parameter is available depending on the device and whether Point Mode is set to Safety Pulse Test . |
Input Delay Time Off -> On | Defines the amount of time for an Off to On transition delay. The input turns on only if the input contact remains on after the on-delay time has elapsed. This prevents rapid changes of the input data due to contact bounce. The default value is 0 ms. |
Input Delay Time On -> Off | Defines the amount of time for an On to Off transition delay. The input turns off only if the input contact remains off after the off delay time has elapsed. This prevents rapid changes of the input data due to contact bounce. The default value is 0 ms. |
Transition Time Limit | Defines the time that the device ignores a discrepancy in input detection so that a slow changing signal does not report a fault. Select a value from 2 ms through 500 ms. Input discrepancy fault reporting is delayed by the value selected. The default value is 100 ms. Transition Time Limit is available for devices with firmware revision 2.011 or later. |
Diagnostics | Opens the diagnostics dialog box for diagnostic information. |
Input Error Latch Time | Defines the time that the input device holds an error to make sure that the controller can detect the error and provide more accurate diagnostics. The valid value ranges from 0 ms through 65530 ms in increments of 10 ms. The amount of time to latch the errors depends on the RPI, the safety task watchdog, and other application-specific variables. The default value is 1000 ms. |
Parameter | Description |
|---|---|
Point | Indicates the point number to which this configuration applies. |
Point Mode | Determines the mode of the test output for the point. The available options depend on the device.
|
Diagnostics | Opens the diagnostics dialog box for diagnostic information. |
Provide Feedback