Points view (input device)

Use the
Points
view to:
  • View a summary of the points for the input device.
  • Configure the input points for the device.
  • Diagnose a problem with an input point.
  • View a summary of the test output points for the input device.
  • Configure the mode of the test output for a point.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal