Test Output diagnostics parameters
The
Ptxx Diagnostics
dialog box includes these parameters:Parameter | Description | Value |
|---|---|---|
Fault exists | Shows whether a fault is present. |
|
Field power | Shows whether field power is present on the point. |
|
Field power on timestamp | Shows the timestamp of the last time field power turned on in YYYY-MM-DD-HH:mm:SS_mmm (UTC-00:00) format.
| A valid time or None if there is no recorded event time. |
Field power off timestamp | Shows the timestamp of the last time field power turned off in YYYY-MM-DD-HH:mm:SS_mmm (UTC-00:00) format.
| A valid time or None if there is no recorded event time. |
Internal fault | Shows whether an internal fault is present. If there is an internal fault, cycle power to the device. If the problem persists, contact Technical Support. |
|
Last fault timestamp | Shows the timestamp of the last internal fault in YYYY-MM-DD-HH:mm:SS_mmm (UTC-00:00) format.
| A valid time or None if there is no recorded event time. |
Short circuit fault | Shows whether an output short circuit or over-current fault is present on the point. |
|
Last fault timestamp | Shows the timestamp of the last output short circuit or over current fault in YYYY-MM-DD-HH:mm:SS_mmm (UTC-00:00) format.
| A valid time or None if there is no recorded event time. |
Overload fault | Shows whether an overload fault is present on the point. |
|
Last fault timestamp | Shows the timestamp of the last overload fault in YYYY-MM-DD-HH:mm:SS_mmm (UTC-00:00) format.
| A valid time or None if there is no recorded event time. |
Provide Feedback