Enterprise Level Dashboard
An enterprise-level dashboard is a powerful tool that offers a unified view of energy performance indicators (ENPIs) and metrics across an organization. By integrating data from various regions and sites, it enables real-time monitoring, analysis, and decision-making. This dashboard empowers executives and managers to track progress, identify trends, and make informed strategic decisions, ultimately enhancing overall business performance.
Click
Enterprise
from the hierarchy list.The following table provides the list of charts available by default in the dashboard:
S.No | Chart/Widget Name | Description |
|---|---|---|
1 | Total Consumption (Harmonized) | This is the overall summary of the total energy consumption. |
2 | Total Costs (Harmonized) | This is the overall summary of the total cost. |
3 | Total Emissions (Harmonized) | This is the overall summary of the resource emission. |
4 | Total Energy Consumption by Site | The user can view the site details on the X-axis and harmonized consumption on the Y-axis. This chart shows the overall energy consumption summary. |
5 | Total Production by Site | This chart shows the overall production summary of site-wise. |
6 | Total Energy Costs by Site | The user can view the site details on the X-axis and the cost on the Y-axis. This chart shows the overall energy cost site-wise. |
7 | Total Emissions by Site | The user can view the site details on the X-axis and the emission on the Y-axis. This chart shows the overall emission site-wise. |
8 | Total Energy Intensity by Site | The user can view the site details on the X-axis and energy intensity on the Y-axis. This chart shows the overall energy intensity summary site-wise. |
9 | Top 5 | The user can view the resource details on the X-axis and attributes (Consumption, Cost, and Emission) on the Y-axis. This chart shows the top 5 resources based on consumption, cost, and emission. |
Refer to Dashboard Features section to manage the Enterprise-Level dashboard.
Related Links
:Provide Feedback