Node Information
FactoryTalk Energy Manager allows its users to view the summary and overall details about that particular node as a tooltip on clicking the
icon beside the node in all the hierarchy levels
icon beside the node in all the hierarchy levels- Name: Name of the node.
- Node Type: Type of the node.
- Currency: Available only for Enterprise and Site.
- Timezone: Timezone of the Site.
- Work Center Type: Type of the selected Work Center.
- Work Unit Type: Type of the selected Work Unit.
For every site/work center/work unit, the
Meter type
and Description
are mentioned along with the Name
in the tooltip.Tooltip/Information Icon

Provide Feedback