Add Enterprise Node
An enterprise-level dashboard is a powerful tool that offers a unified view of energy performance indicators (ENPIs) and metrics across an organization. By integrating data from various regions and sites, it enables real-time monitoring, analysis, and decision-making. This dashboard empowers executives and managers to track progress, identify trends, and make informed strategic decisions, ultimately enhancing overall business performance.
NOTE:
The following points are required to view data on
Enterprise-level dashboard
:- For Cost charts, the respective rate schedule must be configured at the Site level.
- For Emission, the respective emission factor must be configured at the Site level.
- For Production, energy intensity charts must have correct tag mapping for production count measurement.
- For more than one resource meter harmonized unit defined at the Enterprise level can be used for displaying data for consumption, intensity & emission.
- On the left navigation menu, click theSettingsdrop-down and clickConfiguration.Add Node

- ClickAdd Node.TheAdd Nodedialog box is displayed.Add Node

- In theAdd Nodedialog box, provide the following details:
- Name: Provide an Enterprise name.
- Currency: Select a currency from the drop-down list.
- Description: Provide a description of the Enterprise.
NOTE:The user can configure currency at the Enterprise level. - ClickAdd.The "Enterprise added to hierarchy successfully" message is displayed.Enterprise Node Added

Related Information
:Provide Feedback