Add a Preconfigured Device

You can add a preconfigured IO-Link device to your system and use this device configuration across other devices in the system.
We recommend attaching your preconfigured IO-Link device to a new IO-Link master module, or a used IO-Link master module that is restored to the factory default state, to help ensure that the previous device configuration in the IO-Link master module does not overwrite the configuration in the device. Restoring the module to the factory default state clears all device configuration that is stored on all ports from the module.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal