Add IO-Link Devices to Your Project
To add IO-Link devices to your project, you can use the following methods.
IMPORTANT:
You cannot add a device on a channel
that is configured as Fallback if the device does not support standard I/O
mode.
Provide Feedback