Search
PointMax Analog I/O Modules
Analog Output Modules
Analog output modules convert digital values to analog signals. For example, the modules can convert the following:
Volts
Milliamps
Output Module Operation
Data Echo
Rolling Timestamp of Data
Module Data Quality Reporting
Program and Inhibit Mode Handling
Connection Fault Handling
Channel Offset
Hold for Initialization
Output Clamping
Output Ramping Rate Limiting
Field Power (SA Power) Loss Detection
No Load Detection
Short Circuit Detection
Fault and Status Reporting
Calibration
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal