Channel Offset
The Channel Offset feature compensates for any known error on the actuator or channel to
which the actuator is connected. The value is set in the Engineering Units and is added
to the output data.
For example, consider an application that uses the Current (mA) input type with the 4…20
mA range and scaling at 0…100%. If a channel used in the output range 4…20 mA has an
error that results in it consistently outputing 7.8 mA when O.Chxx.Data is 8 mA, you
must account for the error by setting the Channel Offset to 1.25.
Provide Feedback