Replace a Safety I/O Module

Replacing a safety module that sits on a CIP Safety network requires more effort than replacing standard devices because of the safety network number (SNN).
Safety devices require this more complex identifier to make sure that module numbers that are duplicated on separate subnets across all of the networks in the application do not compromise communication between the correct safety devices.
The SNN is a unique identifier that is automatically assigned to each subnet in a safety application. The same SNN is assigned to also devices on the subnet.
However, each safety I/O modules require a unique identifier within the same subnet. A DeviceID is used to uniquely identify each safety module. The SNN and module slot number make up the DeviceID of the safety module.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal