UI session

UI Session is a runtime context in which users execute read or write operations based on permissions.

This section includes

  • UI session overview and presentation engines
  • Idle timeout and screen saver settings
  • UI scaling
  • Locales and localized text
  • Measurement systems and engineering units
  • Time zone options for alarms
  • File download and file upload tracking
  • Session nodes overview

Overview

The UI Session object determines session information, such as the groups to which a user belongs and their locale. Use this information to create dynamic interfaces based on permissions, settings, or custom properties.
An interactive session:
  • Creates the start window for each interactive session.
  • Displays an interactive user interface for the user at runtime.
  • Includes the instances of graphic objects added at design time. Base instances of graphic objects on dynamic navigation logic. Use machine or project global status based on controller status. Use session status for user permissions and session locale. Create the logic through navigation panels, NetLogic, or by displaying and hiding objects.

UI Session and presentation engines

A UI Session generates every time you access an instance of the runtime session. For example, every time you access a web presentation engine, you create an independent session that does not attach to the native presentation engine session. For more information about presentation engines, see Presentation engines.
In the following example, the start pages in the interactive sessions for User1, User2, and User3 are instances of the start page set in the presentation engine.
Each start page includes several instances of the same
A
,
B
, and
C
objects. The objects display or hide based on the dynamic logics for each user. Text translates based on the user locale.
Example: UI Session and presentation engine
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal