Idle timeout
An idle timeout is a configurable period of inactivity in
FactoryTalk Optix
. When no user activity is detected, such as cursor
movements, keyboard actions, or interactions with graphic objects, the application can trigger
a custom event.
TIP:
You can apply idle timeout to a specific screen or an
entire session. To configure an idle timeout, the application must have interactive graphic
objects.
For more information, see:
idle timeout
Provide Feedback