Session nodes
The
{Session}
alias points to the
Session
node for the current runtime session. FactoryTalk Optix Studio
automatically creates dynamic links with the nodes inside of
the Session
node.Node | Description |
|---|---|
Groups | Define and use groups in the project. Each group displays a
value:
|
MeasurementUnits | Display the available units. Each unit includes properties based on
the locale:
|
Locale | Array of session locale IDs. This node specifies all locales
supported by the user interface. |
User | Properties for the user:
|
Roles | Define and use roles in the project. Each role displays a value:
|
Provide Feedback