Create a Project
To start your project, see Create a Project from . You create your project while offline.
TIP:
To import or export a project, see Import a Logix Designer Project or Convert a Project to the Logix Designer Application
from . Incompatibility errors can occur if features exist in the imported project that
FactoryTalk®
Design Studio™
does not support.Provide Feedback