Peer Commands

TIP:
Before you configure peer commands, it is recommended to first add and configure all
EtherNet/IP
In-cabinet system devices in the controller project. The devices must exist in the system before you can define peer commands.
Peer-to-peer communication in an
EtherNet/IP
In-cabinet system allows devices to exchange data directly with each other and perform actions based on their own configuration, without relying on the connected controller.
Once a device is configured to request peer data, the device transmits peer messages to the target devices directly, whether or not they are connected to the controller.
IMPORTANT:
Configuring
CIP Security
and using peer-to-peer communications is not recommended.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal