Add discovered devices
Add the discovered devices the device list and assign them to zones.
TIP:
Discovery
can show multiple child devices under one CIP Proxy device when a security policy is not yet deployed to the CIP Proxy device. After security policy deployment, Discovery
shows only the proxied device as a child.To add a device manually, see Add a device.
Prerequisites
Enable automatic device discovery. See Configure automatic device discovery.
- To add discovered devices
- From the navigation bar, either:
- SelectCanvasand then select a zone orUnassignedto contain the device.
- SelectZonesand then select a zone to contain the device.
- SelectDevicesto contain the device in the devices list not assigned to any zones.
- InDiscovery, select eitherCIPorOPC UA.
- (optional, CIP only) Enable or disableCIP Securityindicators by selecting
Show CIP Security Indicatorsfrom the toolbar.For more information, see Discovery pane. - (optional) Filter the list of discovered devices.For more information, see Search discovered devices.
- Either:
- InDiscovery, select a device or multiple devices and then select.

- InDiscovery, right-click a device and select+ Add.
- Drag a device fromDiscoveryto the table inZonesorDevices.
- Drag a device fromDiscoveryto a zone orUnassignedinCanvas.
The selected discovered devices are added to the zone or unassigned devices list.
Provide Feedback