Search discovered devices
Use
Discovery
to search for a device to determine its location. After the initial discovery of the network topology, you can use filters to limit the scope of the search.When using search, take a note of these functional details:
- Search only examines devices detected or viewed by the browser. Initiating a search will not cause the browser to discover a new device.
- Search queries can contain alphanumeric characters, full words, compound expressions, fragments of a word, or a single letter or number.
- Search includes predefined search criteria to filter search results by device, name, path, and IP address.
- Enclose search queries in quotation marks to find exact matches.
- Use operators in the search query to refine the search results using a logical statement.
- ANDto search for two or more keywords.
- ORto search for several keywords.TIP:An example of using operators between keywords to refine search results is:Device: 1756-L OR Device: 1768-LThis search locates both ControlLogix and CompactLogix controllers.
- Clear the search query to return to the network topology tree view.
- To search discovered devices
- InDiscovery, select eitherCIPorOPC UA.
- (CIP only) From theDiscoverytoolbar, select.
Search - InSearchorFilter, enter a query.
- (optional, CIP only) Select a search filter by selectingto narrow the search results to:

- Device
- The name of the device. For example,1756-L
- Address
- The IP address or a portion of the IP address of the device: For example,10.122.155
- OnlineName
- The online name of the device. For example,Packaging line
- Location
- The communications path used for the device: For example,AB-Eth
Discovery
displays results within a few seconds, regardless of pressing Enter
Provide Feedback