Discovery pane
Use the
Discovery
pane to browse discovered devices and OPC UA
servers and their endpoints, configure networks, and manage drivers.
TIP:
To open or close the
Discovery
pane, select Discovery
from the right toolbar.CIP
Item | Description |
|---|---|
![]() Add | Adds selected CIP devices to the selected zone. |
Auto browse | Continuously discover CIP devices and networks. |
Zoom in | Increases the size of the network topology tree. |
Zoom out | Decreases the size of the network topology tree. |
Search | Toggles Search that provides a filtered list of devices based upon the specified search criteria. |
Settings | Opens advanced network settings. |
Configure Drivers | Adds a driver on the computer to provide communications to a network and configures existing drivers for edit or delete. |
CIP Security Indicators | Show or hide the CIP Security configuration status of a device. |
Indicator | Description |
|---|---|
![]() | The device supports CIP Security and is not yet configured. |
![]() | The device is in the CIP Security configuration process. |
![]() | The device is successfully configured with CIP Security . |
![]() | The device is not recognized. |
![]() | The device configuration process encountered an error. |
(no indicator icon) | The device does not support CIP Security . |
OPC UA
Item | Description |
|---|---|
![]() Add | Adds selected OPC UA devices to the selected zone. |
Auto browse | Verify manually added OPC UA servers and their connection endpoints in the policy model. |
Settings | Opens advanced network settings. |
Discover OPC UA Server | Opens a dialog that enables you to add an OPC UA server and discover its connection endpoints. |
Filter | Provides a filtered list of devices based on the filter query. |
Provide Feedback