Develop a color-coded alarm dashboard

Create a multilingual interface that displays color-coded alarms and enables you to acknowledge and confirm them.
Application example
NOTA:
Download the sample
FactoryTalk Optix Studio
project:
ExampleApplication-ColorCodedAlarmGrid.zip
Prerequisites:
In
FactoryTalk Optix Studio
, select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.
Normal