Configure a localization dictionary

Support a multilingual user interface by configuring the appropriate localization dictionaries.
  1. In the
    Project view
    pane, expand the
    Translations
    folder.
  2. Double-click
    LocalizationDictionary1
    .
  3. Add the it-IT locale.
  4. Translate strings.
    For more information, see Translate a string.
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.
Normal