- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
- NetLogic tutorial
Modified value
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
New value | NewValue | New value inserted within the control. | |
EventId | (Inherited from BaseEventType) | ||
EventType | (Inherited from BaseEventType) | ||
SourceNode | (Inherited from BaseEventType) | ||
SourceName | (Inherited from BaseEventType) | ||
Time | (Inherited from BaseEventType) | ||
ReceiveTime | (Inherited from BaseEventType) | ||
LocalTime | (Inherited from BaseEventType) | ||
Message | (Inherited from BaseEventType) | ||
Severity | (Inherited from BaseEventType) |
Provide Feedback