What's New

Release
: FactoryTalk DataMosaix SaaS 1.02.00

Fixes and Improvements

This release includes the following enhancements:
  • Implemented Accessibility Support for users with disabilities.
  • Creation of custom Groups and Roles (Current release includes only the APIs).
  • FactoryTalk® DataMosaix™
    SaaS APIs are now supported by Machine-to-Machine (M2M) tokens.
  • Multiple roles can be assigned to the Applications and Extractors (M2M). By default, the assigned roles can be changed.
For more information, refer to the online help.

Known Anomalies

  • The scope assignment to a capability is currently limited to
    Datasets
    and
    All
    .
  • Incorrect name appears in the response payload of roles API comprising the claim (group) details. It should show name as
    groups
    , but it is showing name as
    roles
    .
  • While creating a custom role in the current implementation, a user can create a role name that contains only lowercase letters, uppercase letters, numbers, and _ (underscore). In the future release, hyphen (-) and a few other special characters will be supported.
  • Since the token size limit is 8 KB, when a user is part of many groups (irrespective of the tenant, project, or organization counts exceeding 350) the user token fails as its size being greater than the required limit.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal