Release Notes: FactoryTalk DataMosaix SaaS 1.00.02

Fixes and Improvements

This hotfix release includes the following change:
  • With the release of
    FactoryTalk® DataMosaix
    SaaS v1.0.2, the
    FactoryTalk® Edge
    Gateway extractor support is discontinued. All the registered
    FactoryTalk Edge
    Gateway extractors will get deleted once the hotfix v1.0.2 is deployed. This change does not affect the functioning of any other extractor type.

Known Anomalies

  • Create Group button in Cognite Data Fusion (CDF) is enabled despite the user not having capability to create/edit/delete group
    : In the current release of
    FactoryTalk DataMosaix SaaS
    , on the Access Management screen*(Manage > Manage Access > Access Management),*in the CDF portal, the*Create Group button is enabled despite the user not having capability to create, edit, or delete groups.
  • All Admins of
    FactoryTalk® Hub
    organization are not mapped to
    FactoryTalk DataMosaix SaaS
    Project Admin role
    : If a
    FactoryTalk Hub
    organization has multiple Admins, only the Admin or Owner that creates project in
    FactoryTalk DataMosaix SaaS
    is implicitly mapped to Project Admin role in
    FactoryTalk DataMosaix SaaS
    . The
    FactoryTalk DataMosaix SaaS
    other Admins have to be explicitly mapped to the Project Admin role. If the
    FactoryTalk Hub
    Admin that created the project leaves the
    FactoryTalk Hub
    organization, the
    FactoryTalk DataMosaix SaaS
    project will not have any Project Admin, unless other users were assigned to the role explicitly.
  • Access Info in CDF shows all the projects
    : If you click on user name > Access Info link in CDF, all projects existing and deleted are listed irrespective whether the user has access to the project.
  • Clicking on InField menu in CDF gives Insu4cient rights message
    : InField is not supported in the current version.

Previous Releases

Version
FactoryTalk DataMosaix SaaS 1.00.00 - First Release (July 2023)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal