Release Notes: FactoryTalk DataMosaix SaaS 1.00.01
Fixes and Improvements
Fixes and Improvements
This hotfix release included fixes to the following defects:
- The extractors configured inFactoryTalk® DataMosaix™SaaS get deleted sometimes.
- Unable to create Flexible Data Model inFactoryTalk DataMosaix SaaS.
- TheFactoryTalk® Edge™Gateway Extractor sometimes get disconnected from MQTT.
- Unable to connectFactoryTalk EdgeGateway toFactoryTalk DataMosaix SaaSin some circumstances.
- Power BI connector not able to connect toFactoryTalk DataMosaix SaaSproject despite being successfully registered inFactoryTalk DataMosaix SaaS.
Previous Releases
Previous Releases
Version |
|---|
FactoryTalk DataMosaix SaaS 1.00.00 - First Release (July 2023) |
Provide Feedback