Reroot a view
Reroot a view in the network topology tree to limit the view to a selected area in the topology.
FactoryTalk Linx
Network BrowserTo reroot a view
- In the network topology tree in the, select a node in the tree. The anchor appears.FactoryTalk LinxNetwork Browser
- Click the anchor
icon to make the selected row into the new root.In the breadcrumbs area, an anchor icon appears next to the item within the topology where it is anchored. - Click the anchor icon again to return to the normal view.
Fournir une réponse