Bridge across networks
Use a bridge to connect two networks and, if necessary, convert communications from one network protocol to another so that they can communicate. Creating a bridge in the
Network Browser
enables the browser to detect devices on another physical network and enables users to perform diagnostic and configuration functions on those devices. After adding a bridge, the name given to the bridge appears in the Network Browser
tree topology.Fournir une réponse