Module Properties Dialog Box - Power Tab Overview (PowerFlex 700S and PowerFlex 700SE with DriveLogix5720, PowerFlex 700S 2 and PowerFlex 700Se2 with DriveLogix5730, PowerFlex/DPI, SCANPort)

Use this tab to enter power configuration information for the PowerFlex 700S, PowerFlex 700SE, PowerFlex 700S 2, PowerFlex 700Se2, and PowerFlex/DPI, and SCANPort drives. This allows the DriveTools 2000 application to determine the drive type.
Parameters
Firmware Version
Displays the major and minor revision information for the module.
Drive Rating
Lists the ratings provided directly from the Drive Tools application. This listing includes the drive configuration code and any associated configuration text. This information helps to identify the specific drive.
OK
Click this button to accept your edits and close the dialog box.
Cancel
Click this button to cancel your edits and close the dialog box.
Apply
Click this button to apply your edits and continue editing box.
Help
Click this button for help on this tab.
Entregue su opinión
¿Tiene dudas o comentarios acerca de esta documentación? Por favor deje su opinión aquí.
Normal