Rockwell Automation used the latest version of the CVSS scoring system to assess the following vulnerabilities.
CVE-2023-29031 IMPACT A cross site scripting vulnerability was discovered that could potentially allow a malicious user to view and modify sensitive data or make the web page unavailable. User interaction, such as a phishing attack, is required for successful exploitation of this vulnerability.
CVSS Base Score: 7.0
CVSS Vector: CVSS:3.1/AV:L/AC:H/PR:N/UI:R/S:U/C:H/I:H/A:H
CWE: CWE-20 Improper Input Validation
Known Exploited Vulnerability (KEV) database:
No
CVE-2023-29030 IMPACT A cross site scripting vulnerability was discovered that could potentially allow a malicious user to view and modify sensitive data or make the web page unavailable. User interaction, such as a phishing attack, is required for successful exploitation of this vulnerability.
CVSS Base Score: 7.0 (High)
CVSS Vector: CVSS:3.1/AV:L/AC:H/PR:N/UI:R/S:U/C:H/I:H/A:H
CWE: CWE-20 Improper Input Validation
Known Exploited Vulnerability (KEV) database:
No
CVE-2023-29023 IMPACT A cross site scripting vulnerability was discovered that could potentially allow a malicious user to view and modify sensitive data or make the web page unavailable. User interaction, such as a phishing attack, is required for successful exploitation of this vulnerability.
CVSS Base Score: 7.0 (High)
CVSS Vector: CVSS:3.1/AV:L/AC:H/PR:N/UI:R/S:U/C:H/I:H/A:H
CWE: CWE-20 Improper Input Validation
Known Exploited Vulnerability (KEV) database:
No
CVE-2023-29024 IMPACT A cross site scripting vulnerability was discovered that could potentially allow a malicious user to view and modify sensitive data or make the web page unavailable. User interaction, such as a phishing attack, is required for successful exploitation of this vulnerability.
CVSS Base Score: 5.5 (Medium)
CVSS Vector: CVSS:3.1/AV:N/AC:L/PR:L/UI:R/S:U/C:L/I:L/A:L
CWE: CWE-20 Improper Input Validation
Known Exploited Vulnerability (KEV) database:
No
CVE-2023-29025 IMPACT A cross site scripting vulnerability was discovered that could potentially allow a malicious user with admin privileges and network access to view user data and modify the web interface. Additionally, a malicious user could potentially cause interruptions to the availability of the web page.
CVSS Base Score: 4.7 (Medium)
CVSS Vector: CVSS:3.1/AV:N/AC:L/PR:H/UI:N/S:U/C:L/I:L/A:L
CWE: CWE-20 Improper Input Validation
CVE-2023-29026 IMPACT A cross site scripting vulnerability was discovered that could potentially allow a malicious user with admin privileges and network access to view user data and modify the web interface. Additionally, a malicious user could potentially cause interruptions to the availability of the web page.
CVSS Base Score: 4.7 (Medium)
CVSS Vector: CVSS:3.1/AV:N/AC:L/PR:H/UI:N/S:U/C:L/I:L/A:L
CWE: CWE-20 Improper Input Validation
CVE-2023-29027 IMPACT A cross site scripting vulnerability was discovered that could potentially allow a malicious user with admin privileges and network access to view user data and modify the web interface. Additionally, a malicious user could potentially cause interruptions to the availability of the web page.
CVSS Base Score: 4.7 (Medium)
CVSS Vector: CVSS:3.1/AV:N/AC:L/PR:H/UI:N/S:U/C:L/I:L/A:L
CWE: CWE-20 Improper Input Validation
CVE-2023-29028 IMPACT A cross site scripting vulnerability was discovered that could potentially allow a malicious user with admin privileges and network access to view user data and modify the web interface. Additionally, a malicious user could potentially cause interruptions to the availability of the web page.
CVSS Base Score: 4.7 (Medium)
CVSS Vector: CVSS:3.1/AV:N/AC:L/PR:H/UI:N/S:U/C:L/I:L/A:L
CWE: CWE-20 Improper Input Validation
CVE-2023-29029 IMPACT A cross site scripting vulnerability was discovered that could potentially allow a malicious user with admin privileges and network access to view user data and modify the web interface. Additionally, a malicious user could potentially cause interruptions to the availability of the web page.
CVSS Base Score: 4.7 (Medium)
CVSS Vector: CVSS:3.1/AV:N/AC:L/PR:H/UI:N/S:U/C:L/I:L/A:L
CWE: CWE-20 Improper Input Validation
CVE-2023 29022 IMPACT A cross site scripting vulnerability was discovered that could potentially allow a malicious user with admin privileges and network access to view user data and modify the web interface. Additionally, a malicious user could potentially cause interruptions to the availability of the web page.
CVSS Base Score: 4.7 (Medium)
CVSS Vector: CVSS:3.1/AV:N/AC:L/PR:H/UI:N/S:U/C:L/I:L/A:L
CWE: CWE-20 Improper Input Validation
Customers can use
Stakeholder-Specific Vulnerability Categorization to generate more environment specific prioritization.