Safety Partner Status Messages
The safety partner display can show these scrolling messages.
Message | Interpretation |
|---|---|
L8SP | Standard display text. If there is a major nonrecoverable fault, then the fault code scrolls across the display. |
Flash in Progress | A firmware update is in progress. Allow the firmware update to complete without interruption. |
Provide Feedback